This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The Maximum Switching Voltage is the maximum open circuit voltage which can safely be switched by the contacts.
Accordingly, since the Maximum Switching Voltage is 250V AC & DC as mentioned in the Snapshot from the Catalog, thus the contacts could work normally with 125 VDC
Released for:Schneider Electric Egypt and North East Africa