Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to access my HMI through the web ?

Vijeo Designer: WEB Gate remote connection

Vijeo Designer supports a WEB Gate remote connection with any platform which has an Ethernet connection point.
WEB Gate supports remote visualization of Vijeo Designer applications with Internet Explorer on any PC running Windows XP or Windows 7. The size of the page displayed is determined by the terminal.
WEB Gate supports the display of pages similar to those in the Vijeo Designer application, or of different pages, i.e. start-up pages and navigation pages can be differentiated in order to reflect the type of access (terminal/WEB Gate).
Several connections are possible at the same time, with the number depending on the size of the application.
The high security mode of WEB Gate excludes any risk of applications jamming as a result of variables being modified via the terminal and WEB Gate at the same time.

Features Not Available with Web Gate

  • You cannot directly access system variables on Web Gate. However, you can indirectly access system variables by using the Read From Variable and Write To Variable properties.
  • The Toolchest security parts for modifying user account information, such as UserManager and PasswordChange, are not supported on Web Gate.
  • Alarm Summary cursor-related operations such as cursor up/down, page up/down, move top/bottom that are run on the target machine are not reflected on the Web Gate client.
  • In run time, Alarm Banner moves to the back when an error message box appears. But in Web Gate, the Alarm Banner does not change position when an error message box appears.
  • The Alarm Trigger action is not supported on Web Gate for the following functions:
  • Bit
  • Special
  • Popup Panel
  • Script.
  • The following Operations are not supported on the Web Gate client
OperationSupported/Not Supported
System OperationsAll system operations are supported except the following:
ControllerNot Supported
Copy Data To DriveNot Supported
Copy Data From DriveNot Supported
VideoNot Supported
BrowserNot Supported
Image Capture ViewerNot Supported

  • Some script methods are not supported on the Web Gate client. The following table lists the supported and unsupported script methods.
Method TypeSupported/Not Supported
Alarm Group/Category MethodsAll Methods Supported
Java MethodsAll Methods Supported
Alarm Summary MethodsAll Methods Supported
Script Driver MethodsAll Methods Supported
Sound MethodsAll Methods Supported
System MethodsAll Methods Supported except for the following methods:
Variable MethodsAll Methods Supported except for the following methods:
Equipment MethodsNot Supported
Video MethodsNot Supported
File MethodsSupported
DiagBuffer MethodsNot Supported
Recipe Control MethodsAll Methods Supported except for the following method:
  • Actions that run On Shutdown are not supported.
  • Strings that use a font that is not installed on the client PC may appear different from the target machine. Strings are displayed with the closest matching font that is available on the Web Gate client.
  • Popup windows on the Web Gate client always show a titlebar even though the target machine may not use a titlebar.
  • The Video Display is not supported on Web Gate.
  • Printing is not available on the Web Gate client.
  • The web browser's Back, Forward, and Refresh buttons are not supported with Web Gate. Using these buttons may cause errors during run time.
  • Function Key operations assigned to Function Keys on the target can be executed from a client's PC Keyboard through Web Gate, see Section 25.3.4 Simulating the Keyboard for information on how the Function Keys map to a PC Keyboard. The following Function Keys on the PC Keyboard will not run Function Key operations on the target machine:
  • F1 - Displays Web Browser Help
  • F5 - Refreshes Screen
  • F11 - Displays Full Screen
  • Alt + F4 - Closes current window
  • Ctrl + F4 - Closes current tab


-------------------------------------

for more information please refer attachment & Vijeo Designer Help file Section 23.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales inquiry online and an expert will connect with you.

I'd like to receive news and commercial info from Schneider Electric and its affiliates via electronic communication means such as email, and I agree to the collection of information on the opening and clicks on these emails (using invisible pixels in the images), to measure performance of our communications and improve them. For more details, please read our Privacy Policy.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.