{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: What does an SLF3 fault mean on the ATV61 and ATV71 drives?

Issue:
SLF3 fault on the ATV61/ATV71 drives.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Drive is tripping on SLF3 fault.

Resolution:
HMI Com fault is a HMI/ keypad communicating with the graphics display terminal.
Menu 1.6 If the Ref or CMD is set to HMI and if the keypad is disconnected you will trigger a SLF3 HMI coms fault.
Reconnect the keypad and power cycle the drive to clear the fault.

Schneider Electric Egypt and North East Africa