Sepam relay has an ACE969 communications module connected but will not communicate. The ON light is illuminated and no other lights ar lit.
Product Line
ACE969
Resolution
The ACE969 module must be supplied with 24Vdc on both the E1 and E2 terminals and V+ and V-. The power may be jumped between these two sets of terminals. Once the control power is supplied to both sets of terminals (assuming the communication parameters are set correctly) you will now be able to communicate to the Sepam relay.
Released for: Schneider Electric Egypt and North East Africa
Sepam relay has an ACE969 communications module connected but will not communicate. The ON light is illuminated and no other lights ar lit.
Product Line
ACE969
Resolution
The ACE969 module must be supplied with 24Vdc on both the E1 and E2 terminals and V+ and V-. The power may be jumped between these two sets of terminals. Once the control power is supplied to both sets of terminals (assuming the communication parameters are set correctly) you will now be able to communicate to the Sepam relay.
Released for: Schneider Electric Egypt and North East Africa








Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales inquiry online and an expert will connect with you.