{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to enable XML source editing in CET850
Issue
Need to modify a CID file using XML

Product Line
CET850
IEC61850

Resolution
CET850 offers an XML source editor, however it is deactivated by default and must be manually activated.  To activate; open CET850 and click Tools > Preferences. Located beneath Editing Control check the box next to "Enable XML source editing" to activate this feature.

Once this is enabled to view the CID file in XML, highlight the IED click View > Click XML Source.

Schneider Electric Egypt and North East Africa