Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the service breaking capacity and what is the advantage of that on the reliability of breaker?
In a correctly designed installation, a circuit-breaker is never required to operate at its maximum breaking current (Icu). For this reason, a new characteristic has been introduced which is the rated service short-circuit breaking capacity (Ics). IEC 60947-2 expresses (Ics) as a percentage (25, 50, 75, 100%) of (Icu) .

The rated breaking capacity (Icu) or (Icn) is the maximum fault-current a circuit-breaker can successfully interrupt without being damaged. These are very high currents of extremely low probability. In normal circumstances, the fault-currents are considerably less than the (Icu) of the circuit breaker.

On the other hand, (Ics) can be considered as high currents of low probability. It is important that (Ics) be interrupted under good conditions to ensure that the circuit breaker would be immediately ready for re-closure after the faulty circuit has been repaired.

The standard test sequence is as follows: O - CO - CO (at Ics)
Tests carried out following this sequence are intended to verify that the circuit breaker is in a good state and available for normal service.
For domestic circuit breakers, Ics = k Icn where the values for the factor "k" are illustrated on table XIV in IEC 60898.
In Europe, it is an industrial practice to use a k factor of 100% so that Ics = Icu.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more