Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the reference of communication cable of MC-4/11/10/400 Drive which is connected to a diagnostic port with Mini-Din connector ?
The Communication Cable for the Diagnosic Port (MC-4 X7) is 15154304-030,
However the Reference 15154304-030 is obsolete and replaced by the Reference VW3E3057R030, PROGRAMMING CABLE MC 4, 3,0M
Additionally, find attached the Pin Assignment of the Programming Cable (Both cables VW3E3057R030 & 15154304-030 are having the same configuration).
PAC Drive User Manual Page 37
Additionally, Kindly check the Connection Configuration below for the Diagnostic Port (MC-4 X7)
PAC Drive User Manual Page 52
Attachments:
1. Pin Assignment (Steckerbelegung_E-SS-057).pdf
2. PAC Servo Drives MC4 - Operating Manual
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: