{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

what is the rated insulation voltage and the impulse voltage of ACB and switch disconnector NW08 to 63 ?

the rated insulation voltage (Ui) for ACB and switch disconnector NW08 to 63 is 1000 V and for braking capacity (H10 and HA10 ) is 1250 V

the impulse voltage for ACB and switch disconnector NW08 to 63 is 12 KV aslo for braking capacities (H10 and HA10 )

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: