{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.

What is the replacement of XCSZC7902 ?

Reference : XCSZC7902 is Obsolete and it should be combined with reference: XCSZC1 in order to have a complete Coded magnetic switch.
Kindly, Notice that the references combination ( XCSZC7902 + XCSZC1 ) is replaced with XCSDMC7902

Schneider Electric Egypt and North East Africa

Attachment(s)

Preventa_Safety_detection_XCSDMC7902.pdfPreventa_Safety_detection_XCSDMC7902.pdf [62.47 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: