This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
The lifetime of Varplus² capacitors is more than 100,000 hours in respected conditions. But it should be noted that the lifetime of the capacitor greatly depends on the external constraints applied. For example:
- Temperature (an increase of 7°C of the environmental temperature divides the lifetime by 2)
- Presence of harmonics greatly affects the lifetime of the capacitor.
- Temperature (an increase of 7°C of the environmental temperature divides the lifetime by 2)
- Presence of harmonics greatly affects the lifetime of the capacitor.
Released for: Schneider Electric Egypt and North East Africa