{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the Configuration of connecting Twido 24DRF through port 1 with EGX100 gateway on Modbus RTU interface rs485 2 wire.
In that case, the Twido PLC 24DRF used as Modbus Slave & EGX100 RS485 as Modbus Master.
It is possible to use Modbus interface with EGX100 / ETG100 to Twido over Port 1 & port 2 ( Extra Serial Communication adaptor )

1) The communication between the Twido PLC and the EGX100 you need TWD XCA FD010 Communcation cable .
(Refer to attached document for modbus connector pinout of Twido cable TWDXCAFD010.)
Refer to attached document for Twido PLC & TSXETG100 / TSXEGX100 Wiring diagram.

2) You need to Configure Twido Port 1 as 19200, 8 data bits, Even parity, 1 stop bit, Slave Address 1.

3) You try and make a small application with only comm. parameters set - Modbus addr 1 and the above parameters for the line for Port 1.
Refer to attached document for Twido PLC port1 Modbus Communication configuration.
Find attached sample application.


Also do not forget to %MW1000 (for example) to allocate some space for communication experiment - perhaps something like:
|---|%MW100:x0|----------(%M1)--|

Note :-
Port 1 for all Twido compact and modular controllers is a built-in RS485 port, which must be used to communicate to the TwidoSuite programming software. So it has some limitations - not everything you set works on it.
If port 1 is used on the Twido controller, the DPT signal on pin 5 must be tied to the circuit common (COM) on pin 7.
Suggestion: - Kindly used Serial port Adaptor Port 2 for Modbus RS485 communications. (Like TWDNAC485D / T )

4) Configuration of the EGX100.
Refer to attached document for EGX100 Configuration.

Schneider Electric Egypt and North East Africa

Attachment(s)
Twido_TWD XCA FD010.pdf [86.25 KB]
ETG Serial Port Configurtion.jpg [240.57 KB]
My projects.zip [297.19 KB]
Twido Wiring Diagram.jpg [83.83 KB]
EGX100_UserGuide.pdf [3.87 MB]