undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is ADVANTYS STB?
The Advantys STB distributed I/O system is an open, modular input/output system
and makes it possible to design automation islands managed by a master controller
via a bus or communication network.
This distributed I/O system can be used to connect:
·          Motor-starters.
·         Variable speed drives.
·         Magelis® operator interface terminals.
·         Qualified third-party products via the CANopen bus: Festo®, Parker® valves
The Advantys STB I/O family can be divided into 2 groups of modules:
·          Basic modules: A full set of economical network modules and interfaces, with
simplified operating modes.
·          Standard modules: An extended range of input/output modules, with additional
functions: configurable parameters, extended operating modes.
The basic and standard ranges comprise:
·         NIM modules: network interfaces.
·         PDM power distribution modules (c 24 V and a 115/220 V).
·         Input/output modules:

o   Digital I/O (c 24 V and a 115/220 V).
o   Analog I/O, 10, 12 and 16 bit-resolution.
o   Relay outputs (c 24 V coil and c 24 V or a 115/230 V contact)
·         Application-specific I/O module: Counter module.
·         Dedicated modules:
o   for TeSys® Quickfit, TeSys® Model U starter-controllers application.
o   for Tego® Power applications
·         EOS end of segment and BOS beginning of segment modules.
·         External equipment support module on CANopen extension

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: