{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the considerations for running a motor lead longer than a 100 feet on the ATS softstarters?

Issue:
Considerations for running a motor longer than a 100 feet on the ATS soft starters

Product Line:
ATS01, ATS22, ATS480, ATS48

Resolution:
Very long motor cables cause voltage drops due to the resistance of the cable.  If the voltage drop is significant, it could affect the current consumption and the available torque.
This Criteria must be taken into account when selecting the motor and the soft starter.

Ref manual 8636CT0201

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa