{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ION meter data logs are very slow to upload
Issue
Data logs from ION meters are very slow to upload into the ION Enterprise / SPM / PME software.

For devices experiencing this issue the most recent logged data in the database may be several days old even though there is no apparent communication issue with the device.

Product Line
ION Enterprise 6.0.x
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x, 8.x, 9.0, 2020

Environment
Power Monitoring Software

Cause
One possible cause of this issue can happen after deleting register names from ION meter modules in the ION Designer.

In Management Console, access the Diagnostics Viewer Log Performance tab, look at the information for the device that is experiencing this issue, you will see that the event log contains many pending records. The Event Log is always LogHandle 0x1000





















In the Designer application, it is possible to delete the register labels for a module and send those changes to the meter. In the example below the label for Output Register 6 has been deleted.




When this occurs an event will get logged in the meter's event log with the handle value instead of the label name.



Once this happens, the loginserter service will not be able to process the event and the previous event will be the last event logged in the database.

Since there is a high priority on capturing a meter's event log, the other logs on the device may lag behind as the loginserter service is hanging up on the event log.

Resolution
In order to resolve this issue, you will need to clear the meter's event log.

This can be done in ION Setup by modifying a Setup Register in the device's Event Log Control Module which will reset the logged events. You can then revert the change.

Example: Set the Depth to 0 and send the changes then set the depth back to its previous value and send the changes again. The same procedure can be carried out in Designer.





Resetting the Event log will allow the software to begin uploading the Event log successfully.

It is also suggested to add a register label to the module registers that do not have a name.

Schneider Electric Egypt and North East Africa