Issue:
Display a different monitored parameter on an ATV312
Product Line:
ATV312 ATV31
Environment:
All
Cause:
Preference is to normally display a parameter such as motor current or motor torque, not the factory default of output frequency.
Resolution:
Go to SUP menu and display the parameter to be used as a default display ( e.g. LCr or Otr ). Press ENT once to show the current value of that parameter. Then press and hold ENT for about 2 seconds and the display will flash, indicating the process is complete.
Display a different monitored parameter on an ATV312
Product Line:
ATV312 ATV31
Environment:
All
Cause:
Preference is to normally display a parameter such as motor current or motor torque, not the factory default of output frequency.
Resolution:
Go to SUP menu and display the parameter to be used as a default display ( e.g. LCr or Otr ). Press ENT once to show the current value of that parameter. Then press and hold ENT for about 2 seconds and the display will flash, indicating the process is complete.
Released for:Schneider Electric Egypt and North East Africa