{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can I mix C10, C69 with V66 batteries in a Symmetra PX battery frames?

Article available in these languages: Spanish

Issue:
Can I mix C10, C69 with V66 batteries in a Symmetra PX battery frames?

Product line:
Symmetra PX1 & PX2

Environment:
All models/ Serial number

Cause:
APC By Schneider uses multiple vendors to supply the batteries for use in Symmetra PX products. When installing the batteries into the frame they need to be installed in a specific configuration.

Resolution:
If batteries in columns (A and B or C and D) are of two different types, a “mixed battery” fault is generated. You may have two different vendors on the same shelf (level) as long as A&B is the same and C&D are the same. Both the Battery modules and shipping material/packaging are marked with stickers identifying the manufacturer of the batteries. This allows for installing the batteries in such a way as to not generate alarm.

Some common manufacturer of the batteries sticker are; C10, C69, and V66

1Battery levels

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: