Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the suggested cross reference by schneider for ABB thermistor relay CM-MSE?
kindly be informed that we can use one of the 3 thermistors relays according to circuit control voltage :

1-LT3SE00M (PTC probe relay TeSys - LT3 with automatic -reset - 230 V - 1 NC)
2-LT3SA00MW(PTC probe relay TeSys - LT3 with automatic -reset - 24...230 V - 2 OC)
3-LT3SA00M (PTC probe relay TeSys - LT3 with automatic-reset - 115 V - 1 NO + 1 NC

You will find attached datasheets for the this references.
 

Schneider Electric Egypt and North East Africa

Attachment(s)
LT3_LT3SA00M.pdf [50.51 KB]
LT3_LT3SA00MW.pdf [50.46 KB]
LT3_LT3SE00M.pdf [49.39 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: