Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to calculate earth fault loop impedance value (Zs) ?
the Breaker Earth Loop Impedance (Zs) is calculated as follows; Zs = Uo / Ia

Where Uo is the voltage to earth and Ia is the current to trip the breaker in a given breaker disconnection time.

Usually we consider two breaker disconnection times: 5 seconds and 0,4 seconds, depending of the application.

Disconnection time of five seconds is used for fixed equipment. i.e. a machine in a factory or a fixed appliance (electric oven) in a house.

Disconnection time of 0.4 seconds for portable equipment. i.e. power drill or electric lawn mower. This disconnection time is usually used for final circuits (MCB's

A - For a 5 seconds disconnection time
1 - Get to know the voltage to earth (Uo)

2- Determine Ia, see the breaker tripping curve, to find the current needed to trip in 5 seconds (see example on the attached file “Earth Fault Loop Impedance Summary.ppt”, slide 2 and 3)

3- Calculate Zs = Uo / Ia


B – For a 0,4 seconds disconnection time

1- Breakers with electronic trip units – Micrologic (Compact NSb, Compact NSX)

Zs = (Voltage Phase to earth) / (In x Io x Ir x Isd x 1.1)

On some trip units “Io” doesn’t exist, in this case consider Io = 1.

2- Breakers with thermal-magnetic trip units (Compact NS, Compact NB, EasyPact EZC, Compact NSX)

Zs = (Voltage Phase to earth) / (In x Io x Ir x Isd x 1.2)

On some trip units “Io” doesn’t exist, in this case consider Io = 1.