Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the Function of (Y1 slot) in the Connection of the ON-delay timer RE17RAMU?
Y1 = is contact Auxilary for Timers of Functions B or C or ...
The RE17RAMU is of Function (A) starts timing when power is applied directly. The RE17RCMU requires power all the time and is initiated when Y1 to A1 is closed and starts timing when this circuit is opened.
In the case of RE17RAMU, Y1 will not be connected with any terminal as it will not have a clear function.
The RE17RAMU is of Function (A) starts timing when power is applied directly. The RE17RCMU requires power all the time and is initiated when Y1 to A1 is closed and starts timing when this circuit is opened.
In the case of RE17RAMU, Y1 will not be connected with any terminal as it will not have a clear function.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: