{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the equivalent to Control Relays RM4TR31, RM4TR32, RM4TR34 in the RM17/35 range ?
The References RM4TR31, RM4TR32, RM4TR34 are replaced by RM35TF30 (Datasheet of RM35TF30 is attached directly as well).
RM4TR31, three-phase network control relay RM4-T - range 160..220 V
http://www.ops-ecat.schneider-electric.com/ecatalogue/browse.do?cat_id=BU_AUT_528_L3&el_typ=product&nod_id=0000000006&prd_id=RM4TR31
RM4TR32, three-phase network control relay RM4-T - range 300..430 V
http://www.ops-ecat.schneider-electric.com/ecatalogue/browse.do?cat_id=BU_AUT_528_L3&el_typ=product&nod_id=0000000006&prd_id=RM4TR32
RM4TR34, three-phase network control relay RM4-T - range 360 V
http://www.ops-ecat.schneider-electric.com/ecatalogue/browse.do?cat_id=BU_AUT_528_L3&el_typ=product&nod_id=0000000006&prd_id=RM4TR34
RM35TF30, multifunction phase control relay RM35-T - range 194..528 V AC
http://www.ops-ecat.schneider-electric.com/ecatalogue/browse.do?cat_id=BU_AUT_528_L3&el_typ=product&nod_id=0000000006&prd_id=RM35TF30
Attachments:

Zelio_Control_RM35TF30.pdf

Schneider Electric Egypt and North East Africa

Attachment(s)
Zelio_Control_RM35TF30.pdf [80.74 KB]