Issue:
Wondering if you can install both the Ethernet IP and the Ethernet TCP/IP option cards on the ATV61/71 at the same time?
Product Line:
Altivar ATV61 ATV71 with Ethernet TCP IP VW3A3310D or IP VW3A3316 option cards.
Environment:
All
Cause:
Can you have both Ethernet option cards installed at the same time?
Resolution:
No, You can not install the VW3A3310D and the VW3A3316 cards at the same time. You must install one or the other.
Released for:Schneider Electric Egypt and North East Africa