{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is there a roof fan available for the NetShelter SV cabinets?

Issue:
There does not appear to be an optional roof fan for the NetShelter SV cabinets.

Product Line:
NetShelter SV

Environment:
All versions and serial ranges.

Cause:
A request has been made to add a roof fan to a NetShelter SV.

Resolution:
The NetShelter SV cabinets do not currently have roof fans available.
Some of the fans that can be used inside the SV cabinet are: ACF001, ACF002, ACF003, ACAC40001, ACF201BLK, ACF202BLK.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: