{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Can I connect ATV12 to a single phase motor? What are the limitations?
The ATV12 is optimized for three-phase motors due to following limitations:

- Motor winding is not designed to support high drive dv/dt value ( isolation for 50Hz) generated by the PWMI>> Could damage motor in short or medium term.
- Auxiliary winding not designed to support nominal current
- Motor protection not designed to be used with single phase motor >> No protection
- Drive IGBT inverter could be damage also due to the unbalanced current of the motor winding (principal and auxiliary winding have not the same impedancy) >> Could damage product
- Software has not been designed to be used with single phase motor >> Performance not guaranteed

Schneider Electric Egypt and North East Africa