This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
PHF error means : Loss of a line phase
The motor load is too small so the softstarter is sensing phase loss fault
setting On for SSt function and min motor test size 3% from ATS48 capacity .
setting On for SSt function and min motor test size 3% from ATS48 capacity .
Released for: Schneider Electric Egypt and North East Africa