Search FAQs
ATV12 Can you have the run command from remote display and terminals?
Issue:
ATV12 run command in the remote display and the terminals.
Product Line:
Altivar 12
Cause:
Run the drive from 2 command sources
Resolution:
Yes it is possible:
Navigate to ConF- / FULL- / CtL- / FR1 = LCC
Then to CON- / FLO = L1H
This configuration will start the drive from the remote display (the green RUN button) and if we close the contact on LI1.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: