Search FAQs
What can cause an EPHO on an ATV212 drive?
Issue:
EPHO on an ATV212 drive
Product Line:
ATV212
Environment:
All models and serial numbers
Cause:
Loss of one or more output phases
Resolution:
Be sure that you're running a 3-phase motor. Altivar drives cannot be used on single phase motors.
Determine the cause of the missing output phase (such as a bad connection, an output disconnect, or an open winding in the motor), and resolve it.
Check parameter F605 (Output Phase Loss). This should be set to 0 (disabled) if you're using a bypass contactor with this drive. It can also be set to 0 for testing purposes.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: