{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can you adjust the high speed to go above 60Hz on the ATV61 and ATV71 drives?

Issue:
Adjusting the high speed to go above 60Hz on the ATV61 and ATV71 drives

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs to adjust the high speed above 60Hz

Resolution:

WARNING: Setting these parameters too high for your motor could cause motor damage and personal injury. Consult your motor's manufacturer before performing these steps to be sure it's safe for your motor to run above 60Hz and for how long. ​


In the Simply Start Menu 1.1:

  1. Set max frequency (fFr) to to desired value
  2. Set high speed (HSP) to desired value

Schneider Electric Egypt and North East Africa

Attachment(s)
atv61_programming_manual_en_1760649_08.pdf [4.35 MB]