Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
The A and B states of the Quantum Hot Standby CPU's are established based upon MAC address. The lowest MAC address will by default become the "A" CPU. Is it possible to change this behavior?


Yes. During commissioning you can assign the CPU with the higher MAC address to "A" .

  1: Power up the CPU with the higher MAC address.
  2: Using the keypad on the CPU assign the "A" attribute to the CPU.
  3: Download the application to the PLC and issue a start command.
  4: Power up the Standby while holding down the ESC key on the keypad.
  5: When the screen displays "Erasing All RAM wait 2 seconds" let go of the ESC key.
  6: The CPU should become Standby and take on the "B" attribute.

 

R-82917

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: