This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
If error is: New firmware file HID different from Device firmware file HID. ex (in the new Firmware file the HID is 00080008 and the Device Firmware the HID is 000800)
Error Menas :- hardware identification codes are incompatible.
140 CPU53414A Hardware ID and Firmware Operating system file not equal than OS Loader Red Marker on Hardware ID.
1) You can use 140 CPU53414A with Unity Pro or non unity software ( Concept / ProWorX )
2) Kindly First check 140 CPU53414A belongs to which family Unity Pro Or Non Unity Pro.
-- > CPUs with PV < 04 :- Non Unity Pro. kindly use the Conceot :- EXECLoader
CPUs with PV < 04 whose characteristics are not totally adapted to the Unity firmware. kindly use Concept software for Firmware update.
-- > 140CPU53414A >=04 :- Unity Pro
Minimum version required to update Quantum from Concept to Unity: ( Kindly refer Unity Pro Help Modicon Quantum Processors Unity Operating Systems Compatibility Rules )
Attached are the 2 files needed to upgrade your Quantum 140CPU53412A PV=>04 from Concept (or Proworx) to Unity.
I've also attached the Quantum Upgrade Procedure.