Search FAQs
Does the Modbus Plus driver suite work with Windows 2008 Server R2?
Issue:
Is there a version of the Modbus Plus driver that will support Windows 2008 Server R2?
Product line:
Modbus Plus
Environment:
MBX driver software
Cause:
Software not working with Windows 2008 Server R2.
Resolution:
Version 7.1 supports Windows Server 2008 R2 and version 8.0 supports Windows 8 and Windows Server 2012.
As of 1/31/2019 Version 9 of the drivers are out and they support Windows 10.
Is there a version of the Modbus Plus driver that will support Windows 2008 Server R2?
Product line:
Modbus Plus
Environment:
MBX driver software
Cause:
Software not working with Windows 2008 Server R2.
Resolution:
Version 7.1 supports Windows Server 2008 R2 and version 8.0 supports Windows 8 and Windows Server 2012.
As of 1/31/2019 Version 9 of the drivers are out and they support Windows 10.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: