Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
what is the main function for PF ( ready to close contact) in ACB Masterpact NT/NW ?
The “ready to close” position of the circuit breaker is indicated by a mechanical indicator
and a PF changeover contact. This signal indicates that all the following are valid:
  •  the circuit breaker is in the OFF position
  •  the spring mechanism is charged
  •  a maintained opening order is not present:
  •  MX energised
  • v fault trip
  • v remote tripping second MX or MN
  •  device not completely racked in
  • device locked in OFF position
  • device interlocked with a second device.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: