{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the TM2 I/O modules be used on a M221 controller?
Issue:
Using TM2 modules with the M221

Product line:
TM221

Environment:
EcoStruxure Machine Expert Basic (formally SoMachine Basic)

Cause:
Twido obsolete and replacement is the M221

Resolution:
Yes, but the TM2 modules have to be mounted after any TM3 modules if TM3 modules are used.

Schneider Electric Egypt and North East Africa