Search FAQs
Video: How to register an ION service
Issue
An ION Service is removed after installation or does not get installed
Environment
Command Prompt running as administrator
Product
ION Enterprise 6.0
StruxureWare Power Monitoring (SPM) 7.0
Power Monitoring Expert 7.2
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Cause
Many different reasons could cause an ION service to not exist. If the issue is during the installation process it is recommended to contact technical support for assistance.
Resolution
Any of the ION services can be registered from the command line by running:
"-Service"
and unregistered with:
"-UnregServer"
The EXE files are located in \system\bin folder.
Below is an example of registering the OPC service.
Below is a list of the executables associated with each ION service. Not all services are available in each version of the software:
An ION Service is removed after installation or does not get installed
Environment
Command Prompt running as administrator
Product
ION Enterprise 6.0
StruxureWare Power Monitoring (SPM) 7.0
Power Monitoring Expert 7.2
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Cause
Many different reasons could cause an ION service to not exist. If the issue is during the installation process it is recommended to contact technical support for assistance.
Resolution
Any of the ION services can be registered from the command line by running:
"-Service"
and unregistered with:
"-UnregServer"
The EXE files are located in \system\bin folder.
Below is an example of registering the OPC service.
Below is a list of the executables associated with each ION service. Not all services are available in each version of the software:
Service | Executable |
---|---|
ION Alert Monitor | AlertMonitor.exe |
ION Cloud Agent | Cloud.Agent.Pme.Service.exe |
ION Component Identifier | PMLexeMonikers.exe |
ION Connection Management | PMLConnectionManager.exe |
ION Diagnostics and Usage | IONDiagnosticsAndUsage.exe |
ION Event Watcher | IONEventWatcherService.exe |
ION Log Inserter | logsrv.exe |
ION Log Subsystem Router | LogSubsystem.Service.exe |
ION Managed Circuit | LogicalDevice.AutoConfig.ServiceHost.exe |
ION Network Router | PMLNetman.exe |
ION OPC Data Access | ION.OpcDaServer.exe |
ION Power Quality Aggregation | IONPowerQualityAggregator.exe |
ION PQDIF Exporter | PQDIFExporter.exe |
ION Query | QueryServer.exe |
ION Real Time Data | IONServices.exe |
ION Report Subscription | IONReportSubscriptionService.exe |
ION Site | siteserv.exe |
ION Software Alarm or ION Software Data Processing | DataProcessorService.exe |
ION Software Modbus Gateway | ModbusGatewayService.exe |
ION Virtual Processor | vip.exe |
ION XML Subscription | WebReach.XMLSubscriptionService.exe |
ION XML Subscription Store | SubscriptionStore.exe |
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: