The epoxy coating reduces the risk of flash-over (arc) and protects the switchboard and operators against dropped tools, bolts, nuts etc.
- For BlokSeT D, we use epoxy for horizontal and vertical busbar and for all the busbar connections with Masterpact, incoming and outgoing (except Joints).
- For BloksSeT Mf, horizontal, vertical busbar, busbar connection between vertical busbar and NS / NSX / NSXm (line side)
- For BlokSeT Ms and Blokset Dc, only the horozontal and VBB has to be coated with epoxy.
- For BlokSeT Mw2 only HBB can be epoxy coated.
Released for: Schneider Electric Egypt and North East Africa