{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What should parameter bFr be set to if you are using a 50hz 400vac motor?
Issue:
Setting up bFr parameter for a 50hz 400vac motor.

Product Line:
ALTIVAR ATV61

Environment:
All

Cause:
Installation / Setup

Resolution:
Drive settings for bFr, nPr, UnS , nCr and nSP settings,  should match the motor nameplate.
in this case bFr will be set to 50hz and UnS will be set to 400vac

Schneider Electric Egypt and North East Africa

Attachment(s)
atv61_programming_manual_en_1760649_08.pdf [4.35 MB]