{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Download the Vijeo Designer project via File System to a USB stick. It downloaded to the first HMI but not the second one, why?
Issue
Download the Vijeo Designer project via File System to a USB stick. It downloaded to the first HMI but not the second one, why?

Product Line
Magelis XBTG/GH/GK/GT, Harmony HMIGTO/STO/STU, Vijeo Designer

Resolution
The reason is that by default in Vijeo Designer, the Install Option is set for "Single Install".  Which only allows loading the project one time to an HMI.
A system file on the USB stick will then get overwritten and it will prevent download in a second attempt.
Your option would be to set the Install Option to "Multi Install" or rename the file on the USB stick from AGPBAK.SYS to AGP.sys.

Schneider Electric Egypt and North East Africa