{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the HDMPMHKIT27 wiring harness be used to add additional meters to an HDM enclosure?
Issue
A user would like to install additional meters into a HDM meter cabinet.

Product Line
PowerLogic® High Density Metering

Environment
HDM Enclosures Meter Installation

Cause
An auxiliary harness is needed to install additional meters in a HDM enclosure.

Resolution
The Auxiliary Harness Assembly Kit is used when adding a new row of meters to the metering cabinet in the PowerLogic® High Density Metering System.
The auxiliary harness accommodates up to four meters and is used in rows 2, 3, or 4 depending on the number of meters installed and the model of the cabinet.

The Auxiliary Harness Assembly Kit Instruction Bulletin is attached to this article.

Schneider Electric Egypt and North East Africa

Attachment(s)
Auxiliary_Harness_Assembly_Kit_63230-504-203A1.pdf [782.54 KB]