Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Does Schneider Electric have an 8 pole isolator in its portfolio?
When it is referred to 6-pole/8-pole isolator or switch-disconnector, usually what is meant is a set of changeover assembly (2x3P/2x4P). Check the attached image as an example of an 8-pole switch-disconnector (refer to 8 Pole switch-disconnector.png). So upon the rating, you could be directed to the suitable switch-disconnector assembly. For example, for 8P 250A rated isolator, you would be advised to use the attached order form (Compact INS or Compact NSX)
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: