Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the difference between 3P3D and 3P2D NSX breakers?
- 3P2D (3 Poles frame with 2 Poles detection) MCCB has an empty pole, it has only two power contacts inside even if the product looks like a 3P MCCB. 3P2D can be used for single phase applications, to control and protect the phase and neutral.
- 3P3D (3 Poles frame with 3 Poles detection) MCCB is a 3P MCCB and thus it protects its 3 terminals not just 2 terminals
- 4P3D (4 Poles frame with 3 Poles detection) MCCB will protect the 3 phases and won't sense any currents on the 4th pole as the 4th pole does not contain a CT and is not connected to Micrologic and thus won't protect the neutral.
- 4P4D (4 Poles frame with 4 Poles detection) MCCB will protect the 3 phases + Neutral.
- 3P3D (3 Poles frame with 3 Poles detection) MCCB is a 3P MCCB and thus it protects its 3 terminals not just 2 terminals
- 4P3D (4 Poles frame with 3 Poles detection) MCCB will protect the 3 phases and won't sense any currents on the 4th pole as the 4th pole does not contain a CT and is not connected to Micrologic and thus won't protect the neutral.
- 4P4D (4 Poles frame with 4 Poles detection) MCCB will protect the 3 phases + Neutral.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: