Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Is the iC60 range of Acti 9 series UL certified?
The available UL certificate ONLY covers the C60 ranges which belong to the US Multi9 range. The iC60 belongs to the Acti9 range which is not UL certified. If the requirement is to have a multi-standard miniature circuit breaker, then we can offer the global Multi9 multi-standard offer which complies with UL, IEC®, CCC and CSA. This offer is different than the US Multi9 offer.The catalogue for the Multi Standard offer is attached.

Schneider Electric Egypt and North East Africa

Attachment(s)
Multi9 Multistandard Catalogue 2017.pdf [11 MB]
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more