{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the effect of altitude on ATV312?

Issue:
Wondering what is the effect of altitude on ATV312 drives?

Product Line:
All ATV312 and ATV31

Environment:
High altitude, more than 1000m

Cause:
Installing the drive in high altitude above sea level.

Resolution:
For all ATV312, less than 1000m, no derating.
For single-phase supplies and corner grounded distribution networks, up to 2000m, derating 1% per 100m.
For three-phase supplies, up to 3000m, derating 1% per 100m.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV312 Altitude.pdf [77.5 KB]
Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: