Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What is the output voltage from the ATV212 RYA-RYC contact?
Issue:
Needs the output voltage from the ATV212 RYA-RYC contact

Product Line:
Altivar 212 ATV212 

Environment:
All
 
Cause:
Status indication feedback

Resolution:
There is no drive output voltage from the RYA-RYC contact.  This is a dry contact.

Specs are as follows:
Minimum switching capacity: 3mA for 24Vdc
Maximum switching capacity:
   resistive load 3A for 250Vac or 30Vdc
   inductive load 2A for 250Vac or 30Vdc
Maximum response time: 7msec +- 0.5msec

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more