{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the hardware system requirements for a PC to run Vijeo Designer Runtime?
Issue
What are the hardware system requirements for a PC to run Vijeo Designer Runtime?

Product Line
Vijeo Designer

Resolution
The hardware requirements of the Runtime is the same as the Vijeo Designer development.

Platform                      PC
CPU                           Pentium 4 - 2 GHz or faster recommended
Memory                      1 GB minimum, 2GB or more recommended
Available Disk Space   2.0 GB or more on hard disk
Operating System       Microsoft Windows XP Professional (Service Pack 3 or greater)
Microsoft Windows Vista Business edition 32 bits (Service Pack 1 or greater)
Microsoft Windows 7 32 and 64-bit
Microsoft Windows 8.1 32 and 6- bit
Microsoft Windows 10 32 and 64-bit

Schneider Electric Egypt and North East Africa