Issue
What is the maximum number of BCPMs the EGX gateways can have installed downstream?
Product Line
Branch Circuit Power Meter
Environment
BCPM installation
Resolution
EGX Gateways support a maximum of 32 Modbus TCP/IP client connections. Since the BCPM use two modbus addresses it will be able to read up to 16 BCPM units.
What is the maximum number of BCPMs the EGX gateways can have installed downstream?
Product Line
Branch Circuit Power Meter
Environment
BCPM installation
Resolution
EGX Gateways support a maximum of 32 Modbus TCP/IP client connections. Since the BCPM use two modbus addresses it will be able to read up to 16 BCPM units.