Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What is the factory default onboard data logging list of the PM5500?

Issue 
Need to know what data is logged by default on the PM5500. 

Product Line 
PM5500 series meters 

Environment 
Onboard data logs

Cause 
Factory default logged values are not known by customer. 

Resolution 
The PM5500 Series supports onboard logging for up to 14 user-selectable measurements. You can select these measurements as follows: 
d 
The device driver polls the device and checks for new log entries at regular intervals. The default polling interval is 30 seconds.
The polling interval can be modified by changing the value of the register "R3 Poll Period Seconds" in ext_pm5500.ion in the …\system\translators folder. The lowest possible polling interval is 5 seconds.
The measurements available for selection are as follows:

ddd 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: