{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can we monitor the status of the ATV61 drives logic inputs LI1 thru LI5 over the network using Ethernet IP using assemblies 100 and 101?
Issue:
Monitor the status of the logic inputs over the network.

Product Line:
Altivar ATV61 with VW3A3316 Ethernet IP card

Environment:
All

Cause:
Needs to monitor the status of logic input LI5 to see what position the HOA switch is in.

Resolution:
Address 5202 will allow you to monitor the status of the drives logic inputs.  Assign the address 5202 to the communications input table.
Example
Bit 0 is the status of LI1
Bit 1 is the status of LI2
Bit 2 is the status of LI3
Bit 3 is the status of LI4
Bit 4 is the status of LI5
Bit 5 is the status of LI6
Bit 6 is the status of LI7  with Logic IO card installed
Bit7 is the status of LI8   with Logic IO card installed
Bit 8 is the status of LI9   with Logic IO card installed
Bit 9 is the status of LI10  with Logic IO card installed
Bit 10 is the status of LI11  with the extended IO card installed
Bit 11 is the status of LI12 with the extended IO card installed
Bit 12 is the status of LI13 with the extended IO card installed
Bit 13 is the status of LI14 with the extended IO card installed
Bit 14 and 15 are reserved and not used.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: