{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the M580 SD card?
Issue:
Part number for the M580 SD card

Product Line:
M580, EcoStruxure Control Expert


Resolution:
The part number for the SD card is BMXRMS004GPF. Itis optional and is used for applicationbackup and data storage.
Note: This is the only SD card that is compatible with the M580 PAC controllers.

Schneider Electric Egypt and North East Africa