Search FAQs
What is the part number for the M580 weighing module?
Issue:
Part number for the M580 weighing module
Product Line:
M580
Resolution:
The part number for the M580 weighing module is PMESWT0100. Itis a versatile and flexible weighing module controller, which can be used wherever weighing scales are to be used in the Schneider Electric Modicon X80 automation system.
Part number for the M580 weighing module
Product Line:
M580
Resolution:
The part number for the M580 weighing module is PMESWT0100. Itis a versatile and flexible weighing module controller, which can be used wherever weighing scales are to be used in the Schneider Electric Modicon X80 automation system.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: