Search FAQs
How do I protect the project in my M580 PAC?
Issue:
Protecting the project in an M580 PAC
Product Line:
M580 PAC
Resolution:
The input %lr.m.c where r.m.c= rack.module.channel; can be parameterized to protect the internal application RAM and the memory
card as follows:
- %lr.m.c set to 0: The internal application and the memory card are not protected.
- %lr.m.c set to 1: The internal application and the memory card are protected.
*** This is not supported with the M580 Hot Standby controllers ***
Protecting the project in an M580 PAC
Product Line:
M580 PAC
Resolution:
The input %lr.m.c where r.m.c= rack.module.channel; can be parameterized to protect the internal application RAM and the memory
card as follows:
- %lr.m.c set to 0: The internal application and the memory card are not protected.
- %lr.m.c set to 1: The internal application and the memory card are protected.
*** This is not supported with the M580 Hot Standby controllers ***
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: