{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do I configure Vijeo Designer to play sound file on the HMI
Issue:
How to configure Vijeo Designer to play sound file on the HMI


Product Line:
Vijeo Designer


Resolution:
Using Sound methods, you can play sound files (.wav, .daf) on the target machine. You can play one sound file at a time.
Note: Not all target machines support the playing of sound files. Refer to your target machine manual to check if it supports sound files.

1. You will need to add the sound file under the target environment.
2. You can use the system sound method below to play the file.

Methods
Sound.play : Plays the sound file once.
Sound.loop : Repeats playing the sound file.
Sound.stop : Interrupts and stops playing any sound files.

If using scripting to play a file, the string format should be Sound.play( "AliasName" ); where "AliasName" is the alias name given in the sound file editor

Schneider Electric Egypt and North East Africa